Custom Meta Tags
EBV - Solutions - Markets - Transportation and Hirel Animated HB Static HTML
EBV - Aerospace High-Rel Sub Navigation
EBV - Aerospace Main Title (MT)

Aerospace & Defense

EBV - Aerospace - Intro Mixed Media (MM)

Aircraft and space design presents substantial challenges for engineers. Assured operational reliability is essential to ensure lives are not put at risk. The electronic components chosen must therefore be rugged enough that they are able to continue working even when exposed to the harshest application environments such as vibration, shock, or extreme temperatures. To further mitigate the risk of failure, redundancy will often need to be incorporated.

Aerospace Contact EBV (GBL)

Let's talk

Better connected through LinkedIn

Get directly in touch with our Aerospace Director Frank-Steffen Russ

EBV - Aerospace - Icon Table Static HTML
 

Applications & Products

Image of High-Reliability Aerospace Components Icon

High-Reliability aerospace components

Image of Radiation-Tolerant components Icon

Radiation-Tolerant components

EBV - Aerospace - Description Static HTML

 

Space and weight constraints

As well as delivering the highest possible levels of reliability, aircraft electronics hardware cannot take up too much valuable space or impact on payload that can be carried by being too heavy. On this basis, components will be selected that are lightweight and have compact physical dimensions so they can be densely packed together. These limitations will apply to all types of airborne vehicle, but they are even more critical when dealing with UAVs, drones, launchers and satellites.


Emerging trends

Among the key trends in avionics currently is electrification, with an increasing number of electrically-powered aircraft now in the process of being developed. These will call for innovation with regard to the powertrains used, requiring ultra-high efficiency MOSFETs to be employed. The large-scale distribution of monitoring devices throughout new aircraft designs is allowing their structural health to be continuously checked. This means that any indications of possible fatigue can be seen early on - before they become a danger. Based on the same principles, predictive maintenance can be done to replace parts that are coming to the end of their working lives. All this requires sensors for data acquisition, along with accompanying LPWAN wireless communication technology.

Another major trend gaining momentum is ‘New Space’. Instead of missions being restricted just to the established space agencies (like NASA and ESA), lower launch costs have meant that there are now many commercial ventures placing hardware into orbit. The vast majority of these projects will be Low Earth Orbit (LEO) satellite deployments at altitudes below 2000km, rather than deep space missions. A multitude of exciting electronic design opportunities are now being presented, but these require the specifying of appropriate components from a trusted source.


 

Related technical articles

EBV - Aerospace Articles Teaser
How Chip-on-Board Technology is Driving a New Era of Embedded Intelligence
How Chip-on-Board Technology is Driving a New Era of Embedded Intelligence
March 17, 2026
Technical article
Chip-on-Board (CoB) technology integrates dual-band Wi-Fi SoCs directly onto PCBs, enabling compact, efficient, and secure devices. This approach helps engineers build smarter, scalable products across life sciences, smart homes, and beyond.
Read More
view from autonomous vehicle as it interprets street signs
FPGA vs. GPU vs. CPU – hardware options for AI applications
April 7, 2021
Technical article
Field programmable gate arrays (FPGAs) deliver many advantages to artificial intelligence (AI) applications. How do graphics processing units (GPUs) and traditional central processing units (CPUs) compare?
Read More
view from autonomous vehicle as it interprets street signs
Top 10 pitfalls in developing machine vision systems with artificial intelligence
April 7, 2021
Technical article
Machine vision (MV) and artificial intelligence (AI) provide valuable inspection and analysis capabilities to a wide range of leading-edge applications. As with all advanced technologies, there are pitfalls to avoid.
Read More
EBV - Aerospace - Overview Why EBV Static HTML

Why EBV?

Through the unmatched portfolio that we have compiled with our supply partners, EBV Elektronik is perfectly positioned to support customers in both the space and avionics sectors. Our dedicated FAEs have a comprehensive knowledge of these applications and are ready to take you through all the important design considerations. Core franchises here include Broadcom, ISSI, Micron, Microchip, NXP, onsemi and STMicroelectronics. But as well Space specialists like NanoXplore.

We offer an assorted range of high-reliability components. These cover digital ICs including MCUs, SoCs, and FPGAs, communication chips/modules, and advanced sensor solutions, but as well analog and discrete products. So that electronics systems can cope with the radiation issues associated with space deployment, we also supply ICs that are protected from the performance deterioration that radiation can prospectively cause, as well as single-event latch-ups or upsets and other functional errors. The array of radiation-tolerant products offered encompasses memories, processors, data converters and signal conditioning devices. There are numerous other product lines available in relation to these sectors such as the microwave transmitters needed for communication, RF power amplifiers and antennas for use in radar systems, plus GNSS and UWB chips for positioning and navigation tasks.

EBV Aerospace Overview Logo Carousel
Aerospace partners and Space specialists
Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV - Aerospace NPI Product Table
Image Product Description Link New
EBV - Aerospace High-Rel Services (LC)

 

 

Services

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.

Shared Contact EBV Grey (GBL)

Do you have a question?

Contact EBV

If you need any assistance, please click below to find your closest EBV sales office.

EBV - Aerospace NPI Title Static HTML