Custom Meta Tags
EBV - Solutions - Markets - Transportation and Hirel Animated HB Static HTML
EBV - Aerospace - Radiation (SN)
EBV - Aerospace - Radiation Main Title

Radiation-tolerant components

EBV - Aerospace - Radiation Intro (MM)

Once semiconductor devices are deployed into space, they will be subject to cosmic radiation. This can be categorised as being of two different types, with devices needing to be sufficiently screened and tested to show that they exhibit resilience to each of them.

Firstly, there is the total ionizing dose (TID) to consider. Measured in krad, this is an ongoing exposure to radiation resulting from the absorption of energy held by incident charged particles (protons and electrons), which over time will result in a degradation of the device’s performance and shorten its lifespan. If space hardware is only intended to remain functional for a relatively brief period of time, then the TID may not be such a large concern. If, however, this hardware needs to be in operation for several years, then sourcing components that possess higher TID resilience will be important. For LEO deployment, 10krad TID capabilities can be adequate, while for deep space missions, 100krad to 300krad may be needed.

EBV - Aerospace - Radiation Static HTML

The second type of radiation that engineers must be aware of is single event effects (SEEs), for which the measurement unit is MeV.cm²/mg. This is where microelectronic circuitry is hit by a high-energy particle or gamma ray, causing a functional problem to arise. SEEs include single event latch-ups (SELs) that effectively lead to shorts within IC circuitry. In some cases, this will result in permanent damage, but often cycling the device on and off can alleviate the problem. Another type of SEE is single event upsets (SEUs), which can impact upon the integrity of memory devices, resulting in corruption of the stored data.

EBV has an expansive array of radiation-tolerant devices for space deployment. These include microcontrollers and high-density FPGAs, as well as operational amplifiers and diodes, from a variety of different suppliers. It should be noted that we are the only European distributors to support space-grade FPGAs from all the leading programmable logic vendors - meaning that customers have the broadest scope of possible options to choose from.

For certain avionics and space applications, the custom design of an ASIC can be justified - so that the exact performance parameters and functionality can be achieved. Here EBV can support customers in facilitating such projects, liaising with both the customer and the chosen supplier to make the development of high-reliability devices within the required timeframe.

There are also a number of test houses that we can recommend to customers, in order that the certifications can be obtained. Our experienced engineering team can provide design guidance, so that systems are fully prepared to deal with SEEs and appropriate actions can be taken if a chip is affected by them. For SEEs that only cause a short-term sporadic event, it may just require rebooting of that part of the system. If the function is mission-critical though, having redundancy built into the system will be warranted to safeguard against any permanent damage or to take over while rebooting of the main device is conducted. Advice can be given on what diagnostics and monitoring functionality will be needed to check for radiation-related issues arising. Use of linear energy transfer mechanisms, plus inclusion of error correction algorithms, will also have important roles to play in mitigating SEEs.  

 

Aerospace Contact EBV (GBL)

Let's talk

Better connected through LinkedIn

Get directly in touch with our Aerospace Director Frank-Steffen Russ

Design Hub landscape banner Markets Static HTML

 

Design hub landscape banner EBV

 

EBV Embedded Solutions (GBL) grey

Solutions

EBV Embedded Solutions

We're at the forefront of embedded systems innovation, delivering advanced solutions that drive digital transformation across industries.

The Quintessence (GBL) grey

Magazine

The Quintessence

Discover TQ - the free knowledge magazine from EBV

Podcast Spotlight Box (GBL) grey

Resources

EBV Podcast

Our new podcast Passion for Technology is dedicated to the latest technologies, trends and applications in the electronics industry.

Digital Event Hub Spotlight Grid Box Light (GBL)

Resources

Digital Event Hub

See all our on demand webinars and check out our upcoming events.