Custom Meta Tags
Wireless Connectivity Hero Banner

Wireless & Connectivity

ISM 2.4GhZ and Sub-GHz (LC)

ISM 2.4GhZ and Sub-GHz

Azurewave logo
Digi logo
Insight-SiP logo
Nordic logo
Microchip logo
NXP logo
Miromico logo
Qorvo logo
Rohm logo
Semtech logo
STMicroelectronics logo
Renesas logo

ISM radio bands are portions of the radio spectrum reserved internationally for industrial, scientific and medical (ISM) purposes. ISM Bands are license free and not available for Telecomm Applications, which are regulated.

When preparing your application, it is important to note that in some regions the permitted frequencies might differ, e.g. 863 to 870 MHz can be used in Europe and Africa, but in North America 902 to 928MHz is the allowed frequency.

Only some bands are used globally such as the most common ISM Band 2.4GHz to 2.5 GHz used for e.g WLAN and Bluetooth, 802.15.4 is also covered in this section.

Very often we refer to SRD (Short Range Devices) if the Sub-GHz band for data communication is used. The benefit of those Sub-GHz devices is mainly the achieved radio range. Avnet Silica offers mesh networking enabled products based on 802.15.4 in Sub-GHz and 2.4 GHz, as well as simple Sub-GHz transceivers.

Additionally, LoRa, using 868 MHZ, 915 MHz and 2.4 GHz band as well chirp spread spectrum (CSS) modulation can extend the radio range to up to 40 km.

The table below will help you select the most suitable product for your application.

 

ISM Chips Modules 433 / 868 / 915MHz 2.4 GHz LoRa modulation 802.15.4 compliant
(Zigbee / Thread / Matter)
Dual Radio
LoRa and BLE
Concurrent Mode
Zigbee and BLE
Concurrent Mode Thread and Zigbee
Supplier
AzureWave Technologies   ✔   ✔   ✔      
Digi   ✔ ✔ ✔ ✔ ✔      
Insight-SIP   ✔ ✔   ✔   ✔   ✔
Nordic Semiconductor ✔     ✔   ✔     ✔
Microchip ✔ ✔ ✔ ✔ ✔ ✔      
NXP ✔   ✔ ✔   ✔   ✔ ✔
Miromico   ✔ ✔ ✔ ✔        
Qorvo ✔     ✔   ✔   ✔ ✔
Rohm ✔   ✔ ✔          
Semtech ✔   ✔ ✔ ✔        
STMicroelectronics ✔ ✔ ✔ ✔ ✔ ✔   ✔  
Renesas ✔   ✔            

Other technologies (GBL)

Other Wireless & Connectivity Technologies

WiFi (GBLS)

WiFi

Avnet Silica offers a full range of WiFi products, including chips, modules, and devices, as well as a full technology range from WiFi 4 to WiFi 6e. We also support routers and gateways.

SEE WIFI

GNSS (GBLS)

GNSS

Today GNSS technology is not only used for military and cars, but for many types of vehicle, in applications such as container tracking, animal and people tracking and logistics.

SEE GNSS

Antennas (GBLS)

ANTENNAS

Avnet Silica offers antennas from specialised suppliers, that focus solely on antenna design and production, such as Antenova and 2J Antenna, along with other suppliers that offer antennas as part of overall portfolio for wireless products, such as Quectel.

SEE ANTENNAS

Bluetooth (GBLS)

Bluetooth

Bluetooth is one of the most common wireless technologies in the market, propelled into the consumer world by the smartphone, as well as increased demand for fitness, health, and entertainment devices.

SEE BLUETOOTH

RFID (GBLS)

RFID / NFC

Radio Frequency Identification, is a technology that enables simple, secure and fast identification of things, persons and animals. It is mainly made for very short ranges, with one exception, the UHF based RFID called RAIN-RFID for mid range identification, used mainly in logistics.

SEE RFID / NFC

Router (GBLS)

ROUTER / GATEWAYS / MODEMS

Connecting short range wireless devices, or some wired devices to a wired or wireless infrastructure, requires bridging technologies, such as Modems, Gateways or Routers / Access Points.

SEE ROUTERS

Cellular (GBLS)

Cellular

Evolving from GSM to GPRS then to 3G (UMTS / WCDMA) we are now seeing global coverage with LTE / 4G, with next generation 5G leading the way in applications which require higher data transfer.

SEE CELLULAR

UWB (GBLS)

UWB / Ultrawide Band

Ultra-wideband is a radio technology that can use a very low energy level for short-range, high-bandwidth communications (approx. 500 MHz or 20% of the arithmetic center frequency) over a large portion of the radio spectrum. This co-existing with other radio standards is a major advantage.

SEE UWB / ULTRAWIDE BAND

LPWAN (GBLS)

LPWAN

In Europe, major networks have announced their intention not to support 3G networks across Europe beyond 2020. We offer LPWAN technology from our market-leading suppliers, available in a range of modules.

SEE LPWAN

DECT (GBLS)

DECT

Digital Enhanced Cordless Telecommunications, or DECT, was introduced to the market in 1992. It mainly uses the frequency bands 1880 to 1900 MHz, but due to the extension of the ETSI, also 2010-2025 MHz and 24-00 – 2480 MHz are specified.

SEE DECT