Custom Meta Tags
Wireless Connectivity Hero Banner

Wireless & Connectivity

ANTENNAS (LC)

Antennas

2J Antenna logo
Antenova logo
Quectel logo

The quality of a wireless interface mainly depends on the antenna implementation.

Avnet Silica offers antennas from specialised suppliers, that focus solely on antenna design and production, such as Antenova and 2J Antenna, along with other suppliers that offer antennas as part of overall portfolio for wireless products, such as Quectel.

We provide internal and external antenna in various form factors, with different mounting possibilities for many kinds of wireless technologies.

All of our supplier partners, and our specialised suppliers in particular, support integration in the end device with design reviews, pre-testing visibility studies and even pre-certification testing.

Customisation of the antennas is standard practise for Antenova and 2J Antenna, offering a perfectly fitting solution for every wireless system.

 

Antenna Technology Internal Antennas External Antennas Cable & Connector Customization
Cerm. Chip Fiberglass PCB Flex-PCB thru-hole Terminal / Connector mount Screw mount Adhesive Magnetic Wall / Pole mount Automotive
Supplier
2J Antenna ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔
Antenova ✔ ✔   ✔   ✔   ✔         ✔
Quectel Wireless Solutions ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔ ✔     ✔ ✔
Supported Technology Combi WiFi / BT ISM Sub-GHZ UWB Cellular Wide-band GNSS Iridium NFC AM/FM Tetra DVB
Supplier
2J Antenna ✔ ✔ ✔   ✔ ✔ ✔ ✔   ✔ ✔ ✔
Antenova   ✔ ✔ ✔ ✔ ✔ ✔          
Quectel Wireless Solutions ✔ ✔ ✔   ✔ ✔ ✔          

Other technologies (GBL)

Other Wireless & Connectivity Technologies

WiFi (GBLS)

WiFi

Avnet Silica offers a full range of WiFi products, including chips, modules, and devices, as well as a full technology range from WiFi 4 to WiFi 6e. We also support routers and gateways.

SEE WIFI

GNSS (GBLS)

GNSS

Today GNSS technology is not only used for military and cars, but for many types of vehicle, in applications such as container tracking, animal and people tracking and logistics.

SEE GNSS

DECT (GBLS)

DECT

Digital Enhanced Cordless Telecommunications, or DECT, was introduced to the market in 1992. It mainly uses the frequency bands 1880 to 1900 MHz, but due to the extension of the ETSI, also 2010-2025 MHz and 24-00 – 2480 MHz are specified.

SEE DECT

Bluetooth (GBLS)

Bluetooth

Bluetooth is one of the most common wireless technologies in the market, propelled into the consumer world by the smartphone, as well as increased demand for fitness, health, and entertainment devices.

SEE BLUETOOTH

ISM (GBLS)

ISM 2.4GhZ and Sub-GHz

ISM radio bands are portions of the radio spectrum reserved internationally for industrial, scientific and medical (ISM) purposes. ISM Bands are license free and not available for Telecomm Applications, which are regulated.

SEE ISM 2.4GhZ and Sub-GHz

Router (GBLS)

ROUTER / GATEWAYS / MODEMS

Connecting short range wireless devices, or some wired devices to a wired or wireless infrastructure, requires bridging technologies, such as Modems, Gateways or Routers / Access Points.

SEE ROUTERS

Cellular (GBLS)

Cellular

Evolving from GSM to GPRS then to 3G (UMTS / WCDMA) we are now seeing global coverage with LTE / 4G, with next generation 5G leading the way in applications which require higher data transfer.

SEE CELLULAR

RFID (GBLS)

RFID / NFC

Radio Frequency Identification, is a technology that enables simple, secure and fast identification of things, persons and animals. It is mainly made for very short ranges, with one exception, the UHF based RFID called RAIN-RFID for mid range identification, used mainly in logistics.

SEE RFID / NFC

LPWAN (GBLS)

LPWAN

In Europe, major networks have announced their intention not to support 3G networks across Europe beyond 2020. We offer LPWAN technology from our market-leading suppliers, available in a range of modules.

SEE LPWAN

UWB (GBLS)

UWB / Ultrawide Band

Ultra-wideband is a radio technology that can use a very low energy level for short-range, high-bandwidth communications (approx. 500 MHz or 20% of the arithmetic center frequency) over a large portion of the radio spectrum. This co-existing with other radio standards is a major advantage.

SEE UWB / ULTRAWIDE BAND