Custom Meta Tags
Hero Banner
Wide Bandgap (SubNav)
Title and intro (LC)

Five Ways SiC MOSFET Technology Differs from IGBTs

It may seem curious to compare 21st-century silicon carbide (SiC) wide band-gap semiconductor switch technology with silicon-based IGBTs – devices that have been around for over 40 years. However, IGBTs have evolved over time and are still viable and preferred in many applications. In fact, the market for IGBTs is still expanding, with a CAGR of around 10% [1]. 

Substrate (MM)

So, what are the differences that make one or the other technology suitable for a particular design? The Avnet Silica Power Specialists consider five aspects and how they affect your choice.

1. Semiconductor Substrate 

You don’t start your choice of switching device by thinking ‘what substrate’ but the practical characteristics of the base material set the main performance differences. SiC has nearly 3x thermal conductivity, around 10x breakdown voltage for a given thickness and more than 2x the electron saturation velocity of silicon. This means that for a given die size, SiC runs cooler, can be rated to a higher voltage and switches faster, other things being equal. Depending on the end-product design targets, these advantages can be leveraged for better performance, lower cost and/or higher efficiency. 

Silicon carbide macro
Main body and conclusion (LC)

LOOKING FOR SUPPORT? CONTACT OUR POWER EXPERTS

2. Manufacturing Process 

A downside of SiC is the wafer fabrication cost, said in 2021 to be 30-50x for the same size Si wafer used for IGBTs [2], but this can be expected to reduce over time. The effect is offset by the die size – for the same headline performance, a SiC MOSFET die could be around 5x less area than an IGBT. As a material, SiC is more expensive and slower to manufacture and with lower die yield than silicon. SiC wafers are now proven to be viable at 200mm, providing potential further economies of scale, but current production is at the smaller wafer sizes where defect rate is lower. Significantly, IGBT wafers have recently been announced at 300mm, providing further production cost savings for the old technology, offsetting the gains that SiC provides. Factors affecting the relative cost of SiC MOSFETs and IGBTs are very fluid, but it is likely that devices in the new technology like-for-like, will remain significantly higher than IGBTs. When system costs are considered, however, the story can change dramatically, for example, SiC switching at perhaps 10x the frequency of IGBTs can use associated magnetics that are far smaller, lighter and cheaper. 

3. Switching Speed 

Switching speed must be split into two considerations – edge rate and cycle frequency. For sure, both can be dramatically higher in SiC MOSFETs compared with IGBTs, but whether it gives an overall benefit depends on the application. For a given cycle frequency, faster edge rates with SiC reduce transient dissipation or ‘switching loss’. However, EMI is likely to be higher, voltage overshoots higher and layout far more critical. Spurious voltages are generated by high di/dt through trace and wiring inductances which can cause unreliability or even damage, especially if coupled into the gate circuit. High dV/dt can be equally problematic with coupling through device and stray capacitances, for example causing ‘phantom turn-on’ through device miller capacitance. Measures to mitigate all these effects such as adding snubbers and gate protection can add to the cost and size of the end product. Cycle or switching frequency can be higher with SiC than IGBTs, but dynamic losses increase proportionally to a level where there is no advantage over IGBTs. If the benefit of smaller magnetics is leveraged, there can be a large size and weight advantage to high-frequency switching but some applications do not see this – for example motor drives, where the magnetic element is the motor itself. In this application, high frequency and edge rate can be a disadvantage, causing leakage currents, breakdown and bearing wear. 

4. The Gate Driver 

The insulated gates of SiC MOSFETs and IGBTs are nominally similar but practical considerations mean the drive circuits are quite different. IGBTs are very robust, and the drive voltages are not critical – typically +12/15V is used for the on-state with full saturation of the associated bipolar transistor and with a breakdown rating of around +/-30V there is a good safety margin. Both SiC MOSFETs and IGBTs are off for 0V gate drive, but a small negative voltage is sometimes used to counter spurious turn-on from miller capacitance, and voltage transients from common inductance in the gate/emitter loop. An IGBT gate drive can be very simple, just a transformer secondary in some cases. A SiC MOSFET gate, however, needs around +17V for full saturation and this can be alarmingly close to the absolute maximum, which could be around 20/22V. This necessitates close control of the positive drive voltage to avoid damage. Again, a negative gate drive is sometimes actually necessary for the off state because of the high edge rates seen.  

Despite the potential simplicity of an IGBT gate drive, it can sometimes need to provide significant power, proportional to cycle frequency, gate charge and total voltage swing. This can be a watt or more for a large device with a high gate charge. SiC MOSFETS on the other hand have gate charges in the nanocoulomb range and require much less power though if operated at a very high frequency this increases.  

5. Threshold voltage and RDS(on) 

The gate threshold voltage for an IGBT is around 5V and the device can be driven to its full rated collector current with a voltage of around 10V. Higher gate voltages have little effect on collector saturation voltage. In contrast, a SiC MOSFET starts to conduct at perhaps 3V gate voltage but needs 17/18V for full enhancement of the channel. Anything less risks high dissipation and thermal runaway with the positive coefficient of the channel resistance. 

Spot Power (GBL)

Technology

Power: designing solutions with power at the core

We provide you with the right insights and expertise when you need it most, so you can make the right decisions for your product, and your business.

Power - Power components lighting up on board
WBG (CO)

With the ongoing shift to renewable energy and the electrification of transport and industry, the demand for higher power and greater energy efficiency in electronics is increasing. Wide bandgap technologies including SiC and GaN bring many advantages.

WBG OVERVIEW
Conclusion and TH video (MM)

Conclusion 

SiC MOSFETs can outperform IGBTs electrically depending on the application but unit price and system benefits must be considered and costed to evaluate their true worth. Contact the Avnet Silica Power Specialists for comprehensive solutions and expertise to help you make informed decisions tailored to your project's needs. 

References 

[1] https://www.statista.com/statistics/1328255/igbt-market-size/  

[2] https://www.pgcconsultancy.com/post/taking-stock-of-sic-part-1-a-review-of-sic-cost-competitiveness-and-a-roadmap-to-lower-costs  

IGBT vs SiC - Why would you choose one over the other? A snippet from Thomas Hauer's interview with electropages

Working on a project (LC)

Working on a power project?

Our experts bring insights that extend beyond the datasheet, availability and price. The combined experience contained within our network covers thousands of projects across different customers, markets, regions and technologies. We will pull together the right team from our collective expertise to focus on your application, providing valuable ideas and recommendations to improve your product and accelerate its journey from the initial concept out into the world.

WE'D LOVE TO HEAR FROM YOU!

EMEA Power Experts (LC)

About Author

 

Author placeholder image
EMEA Power Experts

We use 'EMEA Power Experts' as a collective byline when our team of power experts and writers collaborate on content.

 

Follow us (GBL)

Like what you see?

Follow us on LinkedIn

Follow our dedicated power page on LinkedIn for the latest power updates and news from our team of power experts.

Modal - Power Contact Us
Contact us

Submit your inquiry via the form below.