Custom Meta Tags
Manufacturer Landing Portlet

XTX Technology

深圳市芯天下技术有限公司(简称“芯天下”)成立于2014年,是一家半导体IC设计高新技术企业。公司于2015年通过ISO 9001质量管理体系认证,2017年被认定为国家高新技术企业、同年获得深创投A轮6000万人民币投资。2018年完成由红杉资本中国基金领投的B轮及国投创业领投的B+轮4.1亿人民币融资。芯天下扎根中国,自主创新,致力于成为卓越的标准芯片设计公司。公司产品规划不仅覆盖了成熟的存储技术路线,而且也已完成未来新型存储器多点布局。目前量产的产品包括SPI NOR Flash, NOR MCP, SPI NAND FLASH, SD NAND FLASH, NAND MCP等,主要应用于物联网,显示与触控,通信,消费电子,工业等领域。服务客户累积超过2500家,包含国内外知名企业。芯天下管理和研发团队均拥有国际存储器知名半导体厂商经验,如飞索半导体、意法半导体、三星半导体、飞思卡尔等。其中,研发人员占比逾60%,公司在现有产品线基础上,不断加大研发力度,着眼于现有成熟技术路线,捕捉AI及5G带来的新的市场机遇,在新型存储器的探索上也已经完成多点布局,研发队伍中来自美国,韩国等海外高精尖人才占比不断提高。团队除了在存储芯片上的垂直深耕,同时也在有序推进标准芯片大方向上的横向扩张,即将在2020年推出通用MCU产品线。芯天下创立之初就确立了“科技创新、芯系天下”的发展使命,并矢志坚持“诚信共赢、开放创新、坚持奋斗、追求卓越”的核心价值观,助力客户迈向卓越的产品表现及价值实现。
Official logo of XTX Technology