Custom Meta Tags
Wireless Connectivity Hero Banner

Wireless & Connectivity

Sub Navigation
RED-DA Compliance main content (LC)

RED-DA Compliance

Information on Avnet Silica's and its suppliers' commitments to RED-DA compliance

An introduction to the new Requirements for Wireless Devices in the EU starting August  2025

The RED-DA (Delegated Act 2022/30/EU to the Radio Equipment Directive) came into effect on August 1, 2025, supplementing the existing Radio Equipment Directive (RED—EU Directive 2014/53/EU) with mandatory cybersecurity requirements. The associated harmonised standards EN 18031-1/-2/-3 were published with limitations in the EU Official Journal on January 30, 2025, and will be applicable from the effective date.

Objective

The objective is to ensure that radio equipment:

  • does not harm the network (Art. 3.3(d)),
  • protects personal data (Art. 3.3(e)),
  • and prevents financial fraud (Art. 3.3(f)).

These requirements apply to end products as well as components (e.g., chips, modules, boards) that can connect directly or indirectly to the Internet. The responsibility lies primarily with the manufacturer of the final product. However, a declaration of conformity may also be required for certain subassemblies.

The three standards

The three standards address different types of devices:

  • EN 18031-1: Radio systems with Internet connectivity
  • EN 18031-2: Data-processing radio devices, wearables, gaming devices, baby monitors, portable radios
  • EN 18031-3: Internet-enabled radio devices used for financial transactions

Devices requiring certification by a Notified Body

Some devices require certification by a Notified Body. Affected categories include:

  • Cellular devices (2G–5G)
  • Wi-Fi and Bluetooth®-enabled devices
  • Radar equipment
  • RFID Devices
  • Televisions and radio receivers

While the EU Commission primarily focuses on end products, there is room for interpretation. According to the EU Blue Guide (2022) and the RED Compliance Association (RED CA), the following clarifications apply and are currently Notified Body practice:

  • Radio Chips, Modules and SOMs, actually require a form of product integration (Antenna integration, Software, Drivers, Protocol Stacks), hence do not qualify as Final Radio Products and therefore are not subject to standalone RED Cyber assessments.
  • Wireless Components (Chips/Modules/SOMs) shipped  as a bare product (i.e., without operating systems or functional application firmware or antenna) are not in scope for RED Article 3.3 (d), (e), or (f) because they cannot:
    • Connect to the Internet directly or indirectly
    • Execute any network-facing behaviour
    • Handle personal data, credentials, or software updates
  • If a Radio Chip or Module includes firmware (e.g., AT command interface, embedded OS and/or Bluetooth stack or special security features supported by ROM bootloader), the decision is on the manufacturer's side, if :
    • The firmware enables Internet connectivity or sensitive data processing out of the box
    • The manufacturer chooses to declare the component as an end product or a subcomponent
  • Modems, routers, and gateways with full software integration must be tested according to RED-DA and provided with a Declaration of Conformity—even if shipped without housing.

Our Wireless & Connectivity suppliers and their commitments to RED-DA compliance

The following overview shows how Avnet Silica’s wireless product suppliers categorise their products and for which types a Declaration of Conformity can be provided.

Ultimately, the manufacturer of the final product placed on the market and the customer are responsible for ensuring RED-DA compliance. 

If you have questions or require a specific DoC from a supplier below, please contact our experts. 

CONTACT OUR WIRELESS & CONNECTIVITY EXPERTS

 

Supplier Product Type WiFi BLE UWB ISM Cellular LPWAN RFID/
NFC
GNSS Summary
Azurewave Modules ✔ ✔   ✔         Not applicable as Azurewave delivers bare modules and not any software.
RED-DA compliance n.a. n.a.   n.a.        
Digi Modules   ✔   ✔ ✔ ✔     Digi's modules with embedded Software conform to RED-DA with DoCs available.
RED-DA compliance         DoC DoC    
  Routers/
Modems
✔       ✔ ✔     Digi's Routers and Wireless Networking Devices conform to RED-DA with DoCs available.
RED-DA compliance DoC       DoC DoC    
H&D Wireless   ✔ ✔             DoC available, even all WiFi modules come w/o software.
RED-DA compliance DoC DoC            
Impinj Chips             ✔   Bare UHF Chips w/o any direct or indirect Internet capabilities.
              n.a.  
Insight SiP Modules ✔ ✔ ✔ ✔   ✔     All products delivered w/o the software and the embedded WiFi product under attestation additionally.
RED-DA compliance n.a. n.a. n.a. n.a.   n.a.    
MaxLinear Chips ✔       ✔       Not applicable as bare chips & software running on the host controller.
RED-DA compliance n.a.       n.a.      
Microchip Chips ✔ ✔ ✔ ✔   ✔ ✔   All MCC Chips are bare chips, and RED-DA is not applicable.
    n.a. n.a. n.a. n.a.   n.a. n.a.  
  Modules ✔ ✔             MCC modules WINCS02PE, RNWF02PE, WINCS02UE and RNWF02UE have a RED-DA attestation, and DoC is provided. All other modules are not subject to RED-DA.
RED-DA compliance DoC DoC            
Miromico Modules       ✔   ✔     Not applicable as modules delivered w/o software.
RED-DA compliance       n.a.   n.a.    
  Gateways/
Router
        ✔ ✔     Gateways will have the RED-DA conformity check until the end of 2025, then DoC will be delivered.
RED-DA compliance         No No    
Nordic Chips ✔ ✔             Not applicable as bare chips & software from OpenSource or customer, but DoC for Dev.-Kits provided.
    DoC DoC            
  Modules         ✔ ✔     DoC for Cellular products provided.
RED-DA compliance         DoC DoC    
NXP Chips ✔ ✔ ✔ ✔     ✔   NXP’s KW45, K32W148, MCX W71 and RW61x wireless MCUs met the compliance to RED-DA and DoCs are available. For host-controlled IW61x, they are also compliant with RED-DA with DoC. All host-controlled devices similar to the IW61x series do not fall under RED-DA. All RFID and UWB products are not able to connect to the internet w/o antenna implementation and serious software and hardware development, RED-DA is not applicable.
RED-DA compliance DoC DoC n.a.          
onsemi Chips   ✔             RED-DA is not applicable to RSL10/RSL15 devices, but relevant on the Module level; therefore, onsemi refers to the module manufacturers regarding RED-DA.
RED-DA compliance   n.a.            
Panasonic Modules ✔ ✔             Panasonic checked their WiFi modules based on RED-DA, confirmed with a DoC on several modules, even if the modules are not capable of connecting to the Internet, hence RED-DA is not applicable.
RED-DA compliance n.a. n.a.            
Qorvo Chips   ✔ ✔ ✔         Bare chips and modules, hence RED-DA n.a., as the customer is responsible for software implementation.
RED-DA compliance   n.a. n.a. n.a.        
  Modules     ✔          
RED-DA compliance     n.a.          
Quectel Modules ✔ ✔ ✔ ✔ ✔ ✔   ✔ Quectel delivered DoCs and Firmware updates for all cellular modules. PCNS informing about the firmware updates have been provided. Quectel delivered DoCs as well for some embedded Wifi and BT modules with integrated software. Host-controlled WiFi modules do not require a DoC as software is not supported.
RED-DA compliance DoC DoC DoC DoC DoC DoC   n.a.
Raytac Modules ✔ ✔             Bare modules hence RED-DA n.a. as customer responsible for Software Implementation.
RED-DA compliance n.a. n.a.            
Renesas Chips ✔ ✔   ✔     ✔   Renesas bare chips are not required to be RED-DA conform, RFID Readers are a matter of EN18031-3 (financial transactions) and will have a RED-DA attestation until the end of October.
RED-DA compliance n.a. n.a.   n.a.     DoC  
  Modules ✔ ✔             As Renesas delivers Modules and also supports Software delivered by Renesas, the DoC for all BLE products is available, and the DoC for WiFi is being prepared at an NB.
RED-DA compliance DoC DoC            
Semtech Chips       ✔   ✔     Bare chips and modules, hence RED-DA n.a.
RED-DA compliance       n.a.   n.a.    
Sparklan Modules ✔ ✔             Bare modules, hence RED-DA n.a. as the customer is responsible for Software Implementation.
RED-DA compliance n.a. n.a.            
STMicroelectronics Chips ✔ ✔   ✔     ✔ ✔ Bare chips do not require a RED-DA certificate.
RED-DA compliance n.a. n.a.   n.a.     n.a. n.a.
  Modules ✔ ✔   ✔ ✔ ✔     All module fully RED certified: - STM32WB5/1 : OK, ST87M01: ongoing , STM32WLM5M01: wip, - ST67W611M1: wip
RED-DA compliance DoC tbd DoC   DoC tbd DoC tbd DoC tbd    
Teltonika Routers/
Modems
✔       ✔ ✔     Teltonika delivered for all Modems, Routers and Gateways with Wireless Connection (Radio) DoCs.
RED-DA compliance DoC       DoC DoC    
Ublox Chips               ✔ Not applicable, as GNSS Chips have no direct connection to the internet.
RED-DA compliance               n.a.
  Modules ✔ ✔     ✔     ✔ For host-controlled modules, RED-DA is not applicable; for embedded modules, u-blox delivered DoC and software updates.
RED-DA compliance DoC              

 

 

Modal - Wireless Connectivity
Contact us

Submit your inquiry via the form below.