Custom Meta Tags
Wireless Connectivity Hero Banner

Wireless & Connectivity

Wireless Connectivity Title Intro (LC)

Wireless technologies evolving future-proof applications

Wireless and Connectivity intro (MM)

Wireless technologies are a key factor in enabling IoT applications both today and in the future, providing connectivity, security and reliability for people and devices. In all kinds of markets and applications, connectivity facilitates the secure the exchange of data, information, voice, and pictures.

It is this connectivity which supports predictive maintenance in industry, monitors energy consumption in Smart Grids, facilitates ambient assisted living for our elderly generation, and ensures security for our families at home. And these are just a few examples.

From Chip and module to complete solutions, including antenna implementation, connectivity, and Cloud services, Avnet Silica has a full portfolio of wireless products to support your design and a team of engineers that can work with you throughout the lifecycle, so that you can be sure your product is future-proof.

CONTACT OUR WIRELESS & CONNECTIVITY EXPERTS

Romain Tesniere of Avnet Silica and Vincent Godel of BICS explain how BICS and Avnet Silica are working together to enable Industry 4.0. Filmed at MWC 2023.

Renesas Wireless Connectivity (MM)

Ultimate connectivity, superior low power performance

Renesas wireless solutions deliver exceptional performance, energy efficiency, and reliable, secure connectivity, from ultra-low-power Bluetooth® Low Energy to advanced Wi-Fi and best-in-class NFC. Whether you're developing a connected home device, Point of Sale terminal, or long-life asset tracker, Renesas provides future-ready wireless built for longevity and scale.

Learn More
NextGenWireless (MM)

Next-Gen Wireless Connectivity

In the ever-evolving landscape of wireless connectivity, staying abreast of the latest advancements is crucial. We delve into the forefront of innovation, spotlighting three key pillars shaping the future of wireless communication: WiFi 6, Bluetooth, and the emergent standard, Matter.

Learn More
Key technologies title (LC)

Key technologies

Static HTML
RED DA Compliance (GBL)

Avnet Silica's RED DA Compliance Information

The RED-DA (Delegated Act 2022/30/EU to the Radio Equipment Directive) came into effect on August 1, 2025, supplementing the existing Radio Equipment Directive (RED—EU Directive 2014/53/EU) with mandatory cybersecurity requirements.

avs-wirless-spotlights-wifi

WiFi

WiFi is the main wireless radio in Local Area Networks. In all kind of markets and applications, this technology is in use for IP-protocol based data exchange, video and voice streaming. Avnet Silica’s portfolio supports WiFi Chips and modules.

5G (GBL)

2G/3G/4G/5G

Since 1991 GSM has been changing electronics and vertical markets fast. Followed by UMTS the demand for higher data transfer speed was leading to a new technology called 4G. Now it is at its limits and 5G is the path to future mobility solutions.

GNSS (GBL)

GNSS

GNSS (Global Navigation Satellite) is the term for all Satellite Localisation Systems including GPS (US), Galileo (EU), Glonass (RUS) and Beidou (CN), used for navigation, tracking and localisation of vehicles, goods and people.

Bluetooth (GBL)

Bluetooth

Bluetooth is the dominating technology for Personal Area Networks. Primarily used for exchanging sensor data and controlling actors, it also enables voice and music streaming. Key applications are in Industry, Consumer, Medical and Smart Home.

LPWAN (GBL)

LPWAN

LPWANs are common for remote monitoring, control and sensing applications. Also used also in predictive maintenance replacing former 2G applications. Wireless technologies NB-IoT, LoRa-WAN, Sigfox and LTE Cat-M are used in LPWAN.

RFID NFC (GBL)

RFID/NFC

NFC, a sub-set of RFID, has increased due to the demand from payment solutions and access control. RFID Chips are most often used in logistic applications, and for identification.

UWB (GBL)

UWB

UWB solutions enable better indoor localisation and tracking in fully automated logistic applications. A key enabler is that the technology is now implemented in Smartphones.

Gateways (GBL)

Gateways

Routers, gateways and modems are the door from Local Networks (LAN/PAN) to the infrastructure via Internet, Cloud, and Intranet. Our broad portfolio of networking components will complete your solution.

DECT (GBL)

DECT

DECT is a technology for Personal Area Network with a focus on telephony. It is dominating the Cordless Phone market. It is also used in some medical, industrial applications and Smart Home applications.

ISM (GBL)

ISM

ISM–band technologies, such as 802.15.4 based Threat and Zigbee, 6LoWPAN, Wirepas and proprietary technologies in Sub-GHz and GHz frequencies, are required where WiFi and Bluetooth are not the right fit, especially Mesh networks.

Cellular Connectivity (GBL)

Cellular Connectivity

A plug-and-play SIM solution for any type of IoT deployment, providing flexible and secure global services and Connectivity for your cellular devices. Our solution works with BICS multi-IMSI profile for reliable access in over 200 countries.

Antennas (GBL)

Antennas

Antennas, are the basis for each RF/Wireless integration. Excellent performance can be achieved with high quality antennas and proper integration.

Modal - Wireless Connectivity
Contact us

Submit your inquiry via the form below.

 
Spot Design Hub Project (GBD)

Tools

Design Hub

Browse and review over a thousand proven reference designs to accelerate your design process. Try our design tool and then export it to your CAD tool of choice.

Spot IoT OLD DO NOT USE (GbD)

Solutions

Internet of Things

Avnet Silica has the perfect supplier offering to enable you to put your product development into the Internet of Things.

Newsletter Subscription (GBD)

Newsletters

Sign up to our newsletters

Join over 10,000 like-minded individuals staying up to date with latest on market trends & insights, products, training opportunities and more!

Customer reading newsletter on tablet.
Contact Us (GBD)

Contact us

Have a question?

Int. Freecall - 00800 412 412 11 | Product or shop-related inquiries: OnlineSupportEU@avnet.com | For anything else, head over to our contact form.