Designing for the IoT as Intelligence Moves to the Edge | Avnet Silica
Designing for the IoT as Intelligence Moves to the Edge | Avnet Silica

Designing for the IoT as Intelligence Moves to the Edge

Smart cars in a crossroad

Discover how to bring your next IoT solution to life with cutting-edge software and hardware from Avnet Silica and onsemi.


The Internet of Everything will be all inclusive, from huge data centers to single-purpose sensors. While individual power requirements vary across the IoT, the need for energy efficiency will be present everywhere.

Spreading IoT intelligence around

IoT is evolving, from a sprawl of raw data sources into focused instances of processed information. Putting intelligence at the edge is creating demand for even more performance using less power and with lower latency. Understanding this, designers and manufacturers are developing and delivering the solutions needed to support doing more with less. Ultra-low power solutions are enabling battery-less designs to be deployed all around the network, each one producing valuable and actionable intelligence.

There are already billions of always-on devices constantly generating and transmitting data over a wider system of networks, feeding cloud-based servers and contributing to Big Data. Power efficiency is relevant at every juncture but the potential to reduce dependency on power is now a reality at the very edge.

Bring your IoT solutions to life with Avnet Silica and onsemi. Learn more here.

If an IoT smart sensor is battery-powered, the TCO (total cost of ownership) goes far beyond the cost of purchase and installation. Every time a battery needs replacing, the owner or operator will incur the cost of an on-site visit. While these can often be scheduled as maintenance, there will always be cases where the battery power fails between routine site visits. The environmental cost of manufacturing and replacing billions of batteries is also significant and for these reasons there is growing interest around developing ultra-low power solutions.

Energy harvesting increasingly viable in the IoT, particularly for ultra-low power sensors

In the past, achieving meaningful communication from harvested energy has been challenging, but through constant innovation, developers now have access to complete wireless sensor reference designs that can operate entirely from harvested energy.

The same approach can be used to design smart sensors using power harvested from solar, motion or temperature differentials. This is made possible by the very low power requirements of the latest devices and is set to enable a wide range of ultra-long battery life or even battery-less smart sensors across the IoT.

Technologies enabling sensing, connection and actuation in the IoT

We have always interpreted the world through sensors; transducers that convert one form of information to another. It could be argued that our five senses are really only transducers, albeit with very high resolution and backed up by the most intensive processor known. If sensors are the eyes and ears of the IoT, actuators are the muscles. The ability to sense a condition, interpret its relevance and act on the results is effectively the value proposition offered by IoT.

The number of ways in which IoT is able to sense, connect and act expands daily. The evolution of sensing technology is truly amazing, spurred on by the opportunity presented by new and exciting applications. One example can be seen in image sensor technology that is empowering vision-based endpoints in IoT, integrating advanced features to cover a wide range of resolutions, dynamic ranges and shutter technologies to address every application.

IoT doesn’t conform to traditional ideas of how technology is used. It is increasingly data-centric and that’s putting new pressures on developers. Data may start with a sensor but it quickly moves to the cloud, so it is now more important to support manufacturers in that entire journey. The right partner can offer just that kind of support — from advice on how IoT can help you, to designing the right solution for your application and adding the cloud services to deliver the insights you’re looking for, all with secure connectivity at the core.

Wireless and wired connectivity is fundamental to IoT and continues to differentiate endpoints. There is no wrong way to connect an IoT node, it all depends on the application. Supporting that takes a product portfolio that covers all of the major solutions, including Bluetooth, Zigbee and Sigfox, as well as proprietary RF implementations in the 2.4GHz and sub-GHz bands. Wired connectivity is still strong in many applications and USB continues to be a popular choice, a position that is strengthened by the emergence of USB Type C.

Actuation is elemental to automation and it invariably involves controlling the application of power, from directing volts to driving motors. The area of power control is synonymous with efficiency, and as  IoT expands it is becoming more important to deliver higher efficiencies at every point.

Reducing design pressure through platforms

Estimates vary but IoT is widely anticipated to comprise tens of billions of devices within the next several years, but what is perhaps more significant is that the revenues expected to be generated by the data produced by the IoT will far outweigh the cost of its implementation.

But even with this clear potential, there is inertia within the industry; this isn’t reluctance to adopt new technologies but rather a resistance to changing the way we work. This can and must be overcome if we are to realize the true potential of IoT.

We can no longer afford to work in isolated pockets of excellence; just as every node is part of something bigger, IoT is multi-disciplinary and also involves multiple groups within organizations. We are actively developing solutions to make this possible, enabling engineers to be more effective designers. 

Turning data into insight

IoT is already a melting pot of protocols and that is only likely to continue to grow. Gateways provide one way of bringing them together, but cloud resources offer greater levels of flexibility and performance. Capabilities like those offered by Avnet’s IoTConnect® Platform deliver convergence between operational and information technology. It offers the ability to connect any number of “things,” with remote access and real-time monitoring, as well as support for moving data between disparate systems. With the IoTConnect Platform, manufacturers tap into a simpler way to address IoT product development.

The opportunity is great and only getting bigger

IoT markets are being defined by companies that can deliver a low-power, data-centric approach to end-to-end connectivity. With many millions of devices already connected and billions more yet to be designed, IoT has a long way to grow. Manufacturers looking to be part of this exciting but challenging opportunity should look for a partner that can add real value to their own design resources, by bringing expertise in all the areas that can make a competitive difference. By working with Avnet Silica and ON Semiconductor, all manufacturers can have the resources, expertise and solutions they need to help them get to market faster.

Learn more about how Avnet Silica and onsemi can enable your IoT applications by exploring our many resources designed to take you from concept to product release.

 

Learn more

Follow Avnet Silica on LinkedIn

Designing for the IoT as Intelligence Moves to the Edge | Avnet Silica
Designing for the IoT as Intelligence Moves to the Edge | Avnet Silica
Related Articles
A factory equipment operator using a transparent control panel showing cyber security
Helping OEMs deliver cyber-resilient products
By Alex Iuorio   -   October 13, 2026
Connected and networked products are potential entry points for cyberattackers.
Smart factory robotics in a car manufacturing plant
From Robots to Production Lines: Why NPUs Are Emerging as the New Standard for Real-Time Industrial AI
By Michaël Uyttersprot   -   September 28, 2026
Industrial robotics and smart factories are increasingly being designed as unified cyber-physical systems.
Designing for the IoT as Intelligence Moves to the Edge | Avnet Silica
Related Events
STMicroelectronics Tech Innovation Day
STMicroelectronics Tech Innovation Day
Date: December 1, 2026
Location: Poland, Gdansk
Microsoft Windows 11 seminar image teaser
Windows IOT Master Image Creation Workshop
Date: November 16, 2026
Location: Multiple locations
Related Designs Menu