Article

Performance under pressure: our new resistive keys are a touch different

Nishant Nishant
resistive keys

In the industrial world, the capacitive touchscreen can be a sensitive soul. It performs beautifully under ideal conditions, but this is a luxury most industries can't afford. So, you can think of our new resistive ‘force-sensing’ technology as its rugged, outdoorsy sibling: ready for a real-world where things just need to get done, regardless of gloved hands, wet surfaces and extreme temperatures.

It’s a ‘force’ to be reckoned with (if you’ll excuse the pun), detecting and measuring the physical pressure applied to a surface, and it’s a completely fresh approach to HMI design. Buttons can be put behind almost any material for the kind of rugged, reliable and safety-critical applications that traditional touch solutions just can’t match.

Where capacitive technology reacts to proximity or moisture, our ‘force-sensing’ solution works with pressure. High-sensitivity sensors sit behind your surface of choice and can detect even the slightest changes when this material is pressed – precise enough to recognize a very light touch (around 100g), even through 0.8mm stainless steel.

In our experience, users notice immediately and it makes a tangible – and very welcome – difference to the way they use the screen:

  • No fingers required. Capacitive screens can be frustrating when you’re wearing gloves or have wet/dirty/sticky hands. Force-sensing technology is totally okay with work gloves, wooden sticks or anything else you’d might find yourself needing to prod a key with. Within reason, of course.
  • Protection from dreaded ‘finger slip’. Because every action needs actual pressure, the chance of an accidental input (sometimes called ‘maloperation’) is significantly reduced. This is especially important for applications like automotive center consoles and active safety systems where unintended inputs can have dangerous consequences.
  • Interference, what interference? Sensors remain fully functional in the presence of water, oil, dust and even electronic noise. Where capacitive keys can struggle with ‘ghost’ touches, there are no such issues with resistive technology.

But in all this excitement, let’s not forget the product designers. This opens up a world of new material options for them, creating huge commercial advantage. Buttons can be hidden behind metal, glass, plastic, wood or even stone. Honestly, there are materials we probably haven’t even considered and that’s great – smoothing the path for exciting new innovations is what we do best.

The upshot is that designers can create products which are more durable and naturally resistant to water and dust without compromising usability and aesthetics. And it’s engineered for the long haul, outlasting traditional mechanical alternatives with a lifespan that exceeds 10 million actuations.

And while you definitely don’t need us to give you ideas of how to use this, we’ve already seen this technology put to elegant use across a number of applications, in particular those where durability and reliability are red lines:

Industrial controls, such as ATMs, coded locks, and outdoor equipment where temperature fluctuations and humidity are everyday design challenges.

In medical & healthcare settings, force-sensing technology is great for creating hygienic, easy-to-clean surfaces for dental equipment and patient monitoring systems.

Safety is the number one priority in the automotive industry, and this technology is perfect for center consoles, door handles and start buttons.

Sleek aesthetics turn smart home appliances from purely functional to distinctive design choices.

Of course, it’s not our place to put the pressure on, but we think this is a solution that is definitely worth getting in contact for. And promise there will be absolutely no more puns when you do.

Our display solutions come in a range of form-factors, and our display experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact Us

About Author

Nishant Nishant
Stefano Rosato, Director, Technical Touch Technology, Avnet

Stefano Rosato is director of technical touch technology in the Display Solutions team at Avnet. Ste...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

Marketing Content Spots
Related Articles
Related Articles
tablet with a PCAP knob
Display on Display: a touch solution that’s instinctively precise and flexible
By Stefano Rosato   -   September 11, 2026
Touchscreens are indispensable to the modern world, but there are situations when we might need something a little more tactile.
Avnet display
Discover the multitool of modules that keeps everyone happy
By Stefano Rosato   -   July 6, 2026
Unprecedented is such an overused word, so it takes a lot for us to choose it when talking about products in our portfolio. However, we took an executive decision on this one, as we believe the TCXD050IBLON-173 5.0-inch TFT-LCD module deserves every  acco...
Related Events
Related Events

No related events found

performance-under-pressure-our-new-resistive-keys-are-a-touch-different