Article

Enabling zonal architectures with high-end MCUs

 generic graphic of person
A modern car with a pcb overlay, showing how vehicles are dependent on electronics
Modern vehicles use zonal architectures to reduce interconnect complexity, improve network efficiency and reduce loom weight.

The move from domain-based to a zonal architecture is primarily a response to mounting complexity, cost and maintenance headaches. The old model, with function-specific ECUs everywhere, turned vehicles into wiring jungles and made updates a real hassle.

Software-defined vehicles are shifting priorities. Instead of hardware dictating features, now it’s software updates driving ongoing functionality. That means OEMs need platforms that are both upgradable and scalable, but also cost-effective.

There’s urgency here.  Avnet is working with its suppliers to help automaker customers navigate those roadblocks. The big technical pain points are the consolidation of ECUs and transitioning from CAN to Ethernet. NXP’s S32 platform offers shared components and software to simplify that journey, so OEMs don’t have to reinvent the wheel every time.

Complexities of SDVs

OEMs underestimated the complexity of moving away from domain-based setups, so delays are mounting. It’s partly about understanding new technology, but also how the pieces fit and making integration easier.

There is a hierarchy in play: central compute, IO aggregators, zone controllers and end nodes. NXP’s S32 portfolio covers every layer, with platform-wide commonality and integration options. That reduces customer effort and helps automakers meet their upgrade and scalability goals, even under cost pressure.

The S32K3’s got scalability up its sleeve, covering devices with a single core up to five ARM Cortex M7 cores, with options for lockstep and split mode. Developers can tailor the processing power to match whatever zone they are targeting without over-engineering, which is a big deal for cost control. Frequency ranges reach up to 320 MHz and flash storage up to 12 MB, with dual bank support for over-the-air updates. There’s networking flexibility, too, with CAN, LIN, FlexIO and up to 1 Gbps Ethernet for automakers wrestling with different protocols.

Safety is fundamental

Automakers are looking for solutions that are ASIL-D ready and ISO 26262 compliant, with hardware security engines, secure OTA and compliance with ISO 21434. That’s crucial as vehicles get more connected.

On the software side, S32K3 ships with production-grade AUTOSAR, non-AUTOSAR and safety packages. Most are complimentary, which directly lowers total cost of ownership. Automakers get a modular, secure and scalable MCU series that makes zonal architecture practical and cost-efficient. That’s a strategic win for anyone aiming to roll out software-defined features without breaking the bank.

NXP sees the S32K389 as the workhorse for zonal tasks where performance and connectivity really matter. It features 12 megabytes of flash, over 2 megabytes of SRAM, plus lockstep and split clock modes. That’s a lot of muscle for aggregating data and keeping latency low. The dual 1 Gbps Ethernet and up to 12 CAN interfaces unlock better throughput and robustness for automakers pushing more real-time communication.

AES hardware acceleration is another layer. It gives direct host code access, so encryption doesn’t bottleneck zonal workloads, especially when striving for compliance for regional standards, like the Chinese cryptographic algorithm.

The advanced S32K3 MCU family from NXP

The advanced S32K3 family from NXP

The S32K3 family spans 512k to 12M onboard flash in packages from 48LQFP 7mm x 7mm to 437MAPBGA 17mm x 17mm (Source: NXP)

System-level integration

Pairing the S32K3 MCU with the FS26 or FS27 power management IC, a high-bandwidth Ethernet switch, and secure CAN with TJA1153 gives you a ready-made backbone for zonal designs. Instead of mixing and matching parts that may or may not play well together, you’re getting a streamlined kit.

That’s a big step toward reducing integration risk. When software enablement and low power modes are already aligned across the stack, you’re cutting out a lot of the usual delays, especially during system bring-up and certification.

Avnet can provide S32K389 and S32K388 evaluation boards and tools to help teams get hands-on, start prototyping and actually validate their setups without waiting for some future release cycle. For OEMs with aggressive launch timelines, those ready-to-order boards are a practical advantage for faster iteration and smoother path to market.

About Author

 generic graphic of person
Miguel Tapia, Transportation Supplier Corporate Account Manager

Miguel Tapia has over 25 years of experience in the semiconductor industry, currently serving as Avn...

Helpful Links

Marketing Content Spots
Related Articles
Related Articles
An electric scooter highlighting the critical electronic subsystems
Targeted solutions for e-mobility’s five critical subsystems
By Miguel Tapia   -   September 28, 2026
From efficient power conversion to connected rider experiences, bringing semiconductors, software, reference designs and system-level platforms together is accelerating e-mobility development.
A wireframe of an electric car showing the battery and key electrical components
How the EV drivetrain is moving toward function consolidation
By Miguel Tapia   -   September 23, 2026
EVs present new opportunities for function consolidation, delivering lower cost and weight, and simpler wiring. But the shift comes with challenges when combining power, control and safety in a single platform. NXP is leading the evolution.
Related Events
Related Events
airplane cockpit looking out on the runway
More Electrification in Aircraft
Date: October 11, 2022
Location: Virtual
satellite in orbit
Space 2.0: AMD Technologies for New Space
Date: February 23, 2022
Location: Webinar
enabling-zonal-architectures-with-high-end-mcus